infrastructure for a connected world

Press Release

Net-Contain™ Universal Aisle Containment System

June 30, 2014, Tinley Park, IL

Panduit Corp., a global leader in Unified Physical InfrastructureSM (UPI)-based solutions, announces the availability of its new Net-Contain™ Universal Aisle Containment System. This versatile system can retro-fit into Brownfield applications or deploy into Greenfield applications to support network, compute or storage containment needs. The system optimizes the separation of hot and cold air to enable higher per cabinet density, reclaiming 10% of existing cooling capacity and saving up to 27% on operational expenses.

The Net-Contain™ Universal Aisle Containment System reduces cooling energy consumption by as much as 40%, can be configured to Hot Aisle or Cold Aisle applications and allows the addition of cabinets of varying sizes and design from different manufacturers, reducing deployment time and capital investment.

“This self-supported containment system reclaims stranded capacity, restores energy efficiency and reduces or defers CapEx by retrofitting an existing data center with an innovative offering of services and environmental monitoring,” said Saurabh Shrivastava, Sr. Manager, Engineering, Corp R & D. “It helps keep the data center cool while keeping costs low, resulting in high reliability. It also provides the flexibility to accommodate current and future data center infrastructure requirements.”

The Net-Contain™ Universal Aisle Containment System features an independent support structure,sliding doors, vertical blanking panels, and ceiling structures for roof containment or wall structures for wall containment. For more information, visit www.panduit.com/universalaislecontainment.

About Panduit:
Panduit is a world-class developer and provider of leading-edge solutions that connect, manage and automate the physical infrastructure. Panduit Unified Physical InfrastructureSM (UPI)-based solutions help customers integrate core business systems for a smarter, unified business foundation. Our robust partner ecosystem, global staff, and unmatched service and support make Panduit a valuable and trusted partner (www.panduit.com).